AOUT#.CUTOFF

Description

AOUT#.CUTOFF sets the cutoff frequency in Hz for a single-pole low-pass filter on the Analog Output.

A value of 0 Hz will turn off the filter and will allow all frequencies to pass through.

The filter can be used with all modes of Analog Output.

Examples

Context

For more information see Analog Output.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write
Units Hz
Range 0 to 10,000 Hz
Default Value 0 Hz
Data Type Float
See Also  
Stored in Non-Volatile Memory Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AOUT1.CUTOFF

3800h

04h

Unsigned32

-

1000:1

Read/Write

No

AOUT2.CUTOFF

3801h

04h

Unsigned32

-

1000:1

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AOUT1.CUTOFF

24100

5E24

Unsigned32

Read/Write

-

AOUT2.CUTOFF

24101

5E25

Unsigned32

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AOUT1.CUTOFF

24100

Float

Read/Write

-

AOUT2.CUTOFF

24101

Float

Read/Write

-